Product Usage

Mechanical power transmission: Movement types, timing belts and gears

There is the uniform movement wherein a body moves at the same speed at all times, and is neither accelerated nor decelerated.

Non-uniform movement occurs when the speed or direction of a body changes during the movement process, which can lead to acceleration or deceleration. There are two cases: uniform acceleration and non-uniform acceleration.

10 Minutes read

Tool for removing pressed-in bearings

A number of things can go wrong during a bearing change: damage to the shaft or bearing can occur due to improper handling or improper installation of the new bearing. Particularly on seized bearings, the question arises as to how to successfully remove the latter without damaging the surrounding components and the bearing itself. In this context, the appropriate tools are crucial for the successful disassembly and installation of pressed-in bearings. In this article, we present tools and methods to ensure that the next bearing change is guaranteed to succeed.

7 Minutes read

Linear motion components - Things worth knowing about guides, screw drives and more

These include linear motors, linear actuators, linear axes, and other components that allow linear motion. Linear motors are specially designed motors that generate linear motion. They generate forces to move loads along a linear track.

10 Minutes read

Ball screw drives - accuracy by preloading

Ball screw drives convert rotary motion into precise linear motion or vice-versa. They are often used as a drive element. Positioning accuracy is critical when using ball screw drives. One way to increase the positioning accuracy of a ball screw drive is to reduce the play between the spindle and nut with a preload. However, since this preload also changes the ease of movement of the system, there are ball screw drives with adjustable preload. The system can be preloaded to such an extent that the permissible axial play between the ball nut and the threaded spindle is achieved without overly limiting the free movement. Preloading can achieve positional accuracy within a few micrometers. In this article, you will learn how this works and what accuracy classes there are.

8 Minutes read

Precise measurements of fitting threads

Precise measurements of fitting threads are crucial for avoiding expensive leaks and system failures. In our blog, you will learn what measuring tools are truly important and which frequent errors you should absolutely avoid when measuring threads. Read more and get valuable tips for error-free joints in your industrial applications.

7 Minutes read

7 steps for selecting a swivel castor

Swivel castors give mobility to objects of all kinds. Mechanical engineering and plant construction, in particular, often require objects to be transported over long distances. Thanks to swivel castors, this is easy and efficient. This article introduces important selection criteria for swivel castors.

10 Minutes read