Types of switches as safety devices in mechanical engineering

Safety switches play an important role in mechanical engineering. They minimize accidents by reliably interrupting or preventing hazardous movements and processes in the event of an emergency. Depending on the application, different types of safety switches are used. This article provides an overview of various safety switches, their functions and their applications.

4 Minutes read

Conveyor technology - Flat belts, conveyor belts and material chutes

Conveyor design and configuration play an important role in material handling. Physical parameters such as the coefficient of friction between the belt and the transport material as well as the surface structure of the transport material determine the maximum inclination angle. This article explains the relevant physical relationships and presents field-proven optimization measures for long-lasting systems.

7 Minutes read

Conveyor technology - Wear indicators of synchronous belts / tolerances of timing pulleys

Synchronous belts or timing belts are installed as drive elements in a wide variety of applications. They are characterized by extremely precise synchronization and efficiency. This feature is used in applications where accurate timing is important, such as positioning tasks or a conveyor belt in the packaging, food or automotive industries. However, it is particularly important in these areas to detect and correct signs of timing belt wear early. In this article, you will learn about the typical signs of wear that occur with synchronous belts and what measures you can use to specifically extend their service life.

8 Minutes read

Correct selection of gearbox synchronous belts

A precisely designed synchronous belt drive is key to efficient and durable power transmission in industrial applications. However, what is important when choosing the right belt? From calculating the rated power to determining the optimum belt width to verifying the center distance between shafts, each step affects the performance and service life of the drive system. Excessive tension can overload components; insufficient tension can cause slippage or tooth failure. That’s why the right belt tension is critical for reliable operation. In this blog post, you’ll learn how to determine the ideal belt configuration step-by-step, which calculation formulas are available to assist you, and what to look for during adjustment and maintenance.

3 Minutes read

Profile connectors for aluminum construction profiles - Accessories

Precisely matched profile connectors are essential for the efficient construction of machine frames, guards and workstation systems. MISUMI’s webshop offers an extensive range of connecting elements that covers various mechanical requirements and profile geometries. What solutions are there and how can they be implemented? In this article, we provide a structured overview of the available variants and their engineering applications.

10 Minutes read

Selecting and replacing the correct timing pulleys, synchronous pulleys, and tensioning rollers

Belt systems are used where mechanical energy must be efficiently transferred. Depending on the specific requirements for power transmission, precision or even noise minimization, different belt profiles and components such as timing pulleys, synchronous pulleys or tensioning rollers are used. This article shows what to look for when making a selection.

10 Minutes read

Aluminum groove profile - Overview and calculation of deflection

Aluminum construction profiles and system profiles act as load-bearing frame profile in mechanical and process engineering. Together with the respective attachments, the aluminum profile forms a stable and lightweight structure for housings and structural and functional tasks. In this article, you will get an overview of available aluminum construction profiles and how to calculate deflection.

12 Minutes read

LX Units - Calculating service life using preselection and calculation tool

Industrial reliability and longevity are key – especially for linear units that operate under high loads and in demanding production environments. But how can you accurately determine the service life of a linear unit? This blog post will show you how to precisely calculate the service life and what factors affect the durability of your systems. Avoid unplanned downtime, optimize your maintenance intervals, and rely on the precise design of your linear components.

19 Minutes read

Reamer bolts and their advantages for an aligned assembly

In many industries, from mechanical engineering to tool making and precision mechanics, the precisely tolerated positioning of components determines the quality and longevity of a product. Conventional threaded joints are often insufficient to precisely align and securely join components. This is where reamer bolts come into play – they ensure a play-free guide in bores and ensure repeatable assembly with the highest precision. In this article, you will learn why reamer bolts are the better choice for aligned joints, and the role of tolerances, thread runouts, and undercuts for optimal assembly.

7 Minutes read

Cylinder pins / tension pins / offset pins - presentation of DIN and ISO standards according to form

Cylinder pins and tension pins are connecting elements for mechanical components. Standards and norms, such as DIN EN ISO 2338 or ISO 8734 for cylindrical pins or DIN EN ISO 8752 for spring pins, define geometry, tolerances, and application areas. Particularly in mechanical engineering, pinning is a reliable method for connecting components permanently and free of play without having to use screw connections. In this article, we look at different forms of connecting pins and their standardization. We also discuss chamfers and surface finishes. In addition, we present differences in standardization and what you need to consider if you want to use pins with different standards.

9 Minutes read

Shaft Couplings and Joints - Compensation of Angular and Radial Offset

In drive technology, flexible shaft couplings and shaft joints are essential to transmit torque between two shafts – especially when the shafts are not exactly aligned or when vibrations and sudden load changes occur in the system. This article explains the difference between shaft joints and flexible shaft couplings, what each component can be used for, and what variants there are.

9 Minutes read

Connectors - Types and applications in industry

Connectors are the invisible backbone of modern industrial equipment – they ensure reliable transmission of power, signals and data. Whether it’s high-performance power connectors, precise signal connections, or highly shielded data connectors, every industrial application has specific material, design, and protection requirements. In this article, we will highlight the different types of connectors, their uses, and what to look for when selecting the right connector.

10 Minutes read

Plugs and connectors for sensor cables

Plugs, connectors, and sensor cables affect the reliability and efficiency of systems in modern industrial automation. But what types of sensors are available and how do you choose the right sensor cable? How is the connection of sensor connectors optimally implemented to ensure secure data transmission? In this blog post, we’ll explore the different connector types, highlight commonly used connectors, and explain some variations of coding M12 sensor connectors – everything you need to know to choose the right connection for your applications.

8 Minutes read

Specialty cables in mechanical engineering - Types of connection, control cables and their applications

In industry, cables and lines ensure safe and efficient signal and energy transmission. But which cable is suitable for which application? Whether it’s a power cable, data cable or hybrid solution, the right choice depends on factors such as flexibility, insulation material, shielding and compliance with (inter)national standards. In this article, we will introduce you to different types of wires and cables in an overview, explain their structure and give you a decision-making aid for selecting wires.

9 Minutes read

Profile Rail Guides - Installation and Maintenance of Linear Guides

How do you achieve the optimum ratio of precision to efficiency when installing and maintaining profile rail guides? In our blog, we highlight different installation methods, explain the difference between mounting and reference surfaces, and provide valuable tips for precise alignment. You will also learn about permissible mounting deviations and how regular maintenance or even maintenance-free concepts can affect the service life of your linear guides.

9 Minutes read

Profile Rail Guides - Allowable Loads of Linear Guides

In the industrial environment, precision and reliability count – especially for profile rail guides used in demanding conditions. But how are permissible loads calculated correctly to minimize the risk of failure while maximizing efficiency? In our blog, we explain the key calculation variables such as dynamic and static load capacity and provide insights into the distribution of forces and moments. Benefit from in-depth expertise that helps you design your applications.

16 Minutes read

Safety screws - Tamper-proof screws

Screw connections can be detached independently or detached without authorization by third parties. In order to prevent this, so-called Safety screws have been developed that make it difficult or impossible to manipulate screws. In addition to safety screws with special screw heads, there are also other design options. In this article you will find everything necessary to protect your screw connection from theft or tampering in the future.

8 Minutes read
Lightweight pneumatic coupling for PU hoses
Lightweight pneumatic coupling for PU hoses

Pneumatic Couplings and Pneumatic Pipe Fittings

Pneumatic couplings are used in pneumatic systems to connect and disconnect hoses and pipes. What types of pneumatic couplings or Which quick connectors are available, whether they are compatible with each other, and which hoses can be connected to them, you can find out in this article. In addition, the assembly and aspects of occupational safety are discussed, since there is sometimes very high pressure in pneumatic systems.

12 Minutes read

Profile Rail Guides - Calculation of the Service Life of a Linear Guide

In industrial automation and mechanical engineering, profile rail guides are the backbone of precise and efficient motion. But how long do they really last – and what factors affect their lifespan? Read our blog to learn which types of service life are relevant, the advantages and disadvantages of profile rail guides, and how to maximize the service life of your equipment through precise calculations and targeted optimizations. Read on to learn how to make careful decisions to avoid operational downtime and ensure long-term productivity.

11 Minutes read

Linear Systems - Stability and precision by combining linear units with linear guides

In modern production and automation systems, precision and stability are critical to quality and efficiency. The right combination of linear units and linear guides not only optimizes motion accuracy, but also increases system rigidity, durability, and load capacity. In this blog, we’ll explore how you can improve the performance of your machines through the targeted selection and integration of linear units and additional guides – from optimal sizing to load sharing concepts to practical implementation strategies for demanding industrial applications.

11 Minutes read