Ideal and deviating shaft diameter
Ideal and deviating shaft diameter

Linear shafts: Precision standards for MISUMI linear shafts

Linear shafts are a subset of linear guides and provide stability and precision in linear motion systems. Varying precision requirements are placed on linear shafts to ensure that movements are transferred at low-friction, accurately, and reliably. These requirements specify roundness, straightness, perpendicularity as well as the concentricity of the linear shaft. MISUMI offers linear shafts in standard and precision versions. In this article, you will learn about the different features, when to use which variant, and what precision requirements are all about.

11 Minutes read

Linear shafts: Selecting the right material, hardening, and surface treatment

Linear shafts perform demanding tasks in industrial applications: They permit precise and repeatable linear movements under high mechanical loads. To meet these requirements, proper material selection, hardening, and surface treatment is critical. All of these factors directly affect the service life, precision and performance of a linear shaft. This article introduces these three aspects and highlights their dependencies so you can select the best linear shaft for your application.

11 Minutes read

Linear ball bearings – Selection, installation and maintenance

Linear ball bearings are important components in many mechanical engineering applications. The function of linear ball bearings is to enable precise and low friction movement along an axis. This article provides important guidance on the selection, installation and maintenance of linear ball bearings, so you can be sure to find the right bearing for your application and get the most out of it.

11 Minutes read

Ball bearings – Load distribution for rolling bearings

Ball bearings and other rolling bearings are installed in numerous machines. The installed bearings transfer the radial or axial forces that occur to the machine housing and thus permit the use of various moving components. The forces that occur and the resulting load in the bearing must already be determined during the design process. The load distribution in the bearing and the matching contact point geometry is crucial for the expected service life, function and efficiency of the bearing. In this article, we will look at the load exerted on a rolling bearing and how contact surface geometry affects load distribution in the rolling bearing.

10 Minutes read

Pipe Fittings – Types and applications

Pipe fittings are used to securely connect pipes, tubes, and hoses. They are used in pneumatics as well as in hydraulics and other fluid-carrying systems. However, suitable fittings and adapters are also available for pipes under vacuum. As an important component of these systems, it is essential that pipe fittings reliably and securely connect the components to be connected and permanently prevent liquids or gases from entering or exiting. This article introduces different types of pipe fittings and their ideal uses, and will help you choose the best pipe fitting for your application

10 Minutes read

Specialty plastics for practitioners – Properties, resistance and application examples

Specialty plastics are used when applications place high demands on the material or special properties are required. They frequently have insulating properties and their high resistance to water and chemicals makes them a reliable, low-maintenance material. It is then no wonder that specialty plastics are used in many technical fields and also in fasteners such as screws and nuts. The following article provides an overview of various specialty plastics and their applications.

12 Minutes read

Neodymium magnets: Special features, production and uses

Neodymium magnets are the strongest permanent magnets available and can produce very strong magnetic fields in the smallest of spaces. This property allows them to be integrated into a variety of devices and applications even when space is limited.

What makes neodymium magnets so strong, what applications are available, how they are made, and what to consider when using them is discussed in this article.

9 Minutes read

Cleanrooms and cleanroom technology – Global differences in standards

Controlled environments such as cleanrooms are essential to maintaining product quality, safety and standards in many industries. In semiconductor manufacturing, for example, even the smallest particles can damage the sensitive surfaces or lead to undesirable chemical reactions. But what defines a cleanroom? What conditions must be met and what classes are there? And what cleanroom technology can be used to implement cleanrooms? The following article introduces the concept of cleanroom in more detail, including addressing these questions and standards worldwide.

13 Minutes read

Parallel keys and tapered keys – Standards and norms (OLD+URL Redirect)

Parallel keys and tapered keys are two common connecting elements in the mechanical engineering industry. They are used to create a force-locking connection between two components. In this article, the two key types are examined in more detail and their areas of application are explained.

1 Minutes read

Machining of stainless steels

Stainless steel is a material that is difficult to machine. Machining entails a risk of cold tempering. In addition, machining errors can create attack surfaces for corrosion. The following article answers the frequently asked question "Can stainless steel rust?", provides an overview of problems during machining, various machining methods and selection criteria for the correct tool for machining stainless steel.

10 Minutes read

Tool for removing pressed-in bearings

A number of things can go wrong during a bearing change: damage to the shaft or bearing can occur due to improper handling or improper installation of the new bearing. Particularly on seized bearings, the question arises as to how to successfully remove the latter without damaging the surrounding components and the bearing itself. In this context, the appropriate tools are crucial for the successful disassembly and installation of pressed-in bearings. In this article, we present tools and methods to ensure that the next bearing change is guaranteed to succeed.

7 Minutes read

Antistatic Materials - ESD - Definition and Benefits

Electrostatic discharge can be a problem in the manufacturing environment: the hazards range from damage to sensitive components to fire and explosion hazards. There are a variety of options for minimizing its occurrence. Antistatic or ESD materials are one of them. The following article covers causes for electrostatic charge, introduces antistatic materials (ESD materials), and describes general principles for avoiding electrostatic discharge.

9 Minutes read
Sensor integrated into the overall system
Sensor integrated into the overall system

Sensors - selection and importance for automation technology

Collecting data is a central aspect of modern facilities, especially in the context of digitalization and Industry 4.0. Sensors make this possible. They provide input data and monitor and adapt processes. But what types of sensors are there? How does one select the right sensor for a specific application? This article presents the mode of action and possible applications for various sensors, as well as selection criteria for finding the right sensor.

8 Minutes read

Dial gauges - Types and Properties

Dial gauges are indispensable for industrial manufacturing – they ensure precision and quality in various technical processes. In our blog, we highlight their importance and present the different types of analog dial gauges, and digital and inductive gauges. We will take a look at modern alternatives and explain how dial gauges are used in manufacturing for tolerance control, machine adjustment and quality inspection. Find out how these measuring instruments improve efficiency and accuracy in industry.

8 Minutes read

Understanding rotary shafts, axes, and motor shafts: A guideline

Rotary shafts are an essential element of modern mechanical engineering. Rotary shafts transfer rotary motion. They can be manufactured from different materials, which are selected specifically to match the application. The materials include stainless steel, corrosion-resistant steel, and steel.

5 Minutes read

Ball screw drives - accuracy by preloading

Ball screw drives convert rotary motion into precise linear motion or vice-versa. They are often used as a drive element. Positioning accuracy is critical when using ball screw drives. One way to increase the positioning accuracy of a ball screw drive is to reduce the play between the spindle and nut with a preload. However, since this preload also changes the ease of movement of the system, there are ball screw drives with adjustable preload. The system can be preloaded to such an extent that the permissible axial play between the ball nut and the threaded spindle is achieved without overly limiting the free movement. Preloading can achieve positional accuracy within a few micrometers. In this article, you will learn how this works and what accuracy classes there are.

8 Minutes read

Linear motion components - Things worth knowing about guides, screw drives and more

These include linear motors, linear actuators, linear axes, and other components that allow linear motion. Linear motors are specially designed motors that generate linear motion. They generate forces to move loads along a linear track.

10 Minutes read

Properties of plastics – Which plastics are suited for mechanical engineering?

Technical plastics are an indispensable part of modern industry. In custom machine construction in particular, they find a wide range of applications because they have a high degree of flexibility and formability. It is important to know what properties plastics must have in components and standard parts in custom machine construction. This article describes the most important applications for plastics in mechanical engineering.

4 Minutes read

Tutorial: Modulus of elasticity of steel – Materials science

Steel is an important material in modern industry and is used for a variety of applications. A crucial property to consider when using steels is their elasticity. The modulus of elasticity or Young’s modulus indicates how much stress is needed to achieve a certain degree of elongation. In this article we will look at the different types of steels and their respective elastic moduli.

5 Minutes read