Lubrication of Ball Screw Drives – Lubricants, Application Areas and General Information

Ball screws drives or recirculating ball spindles should never be used without lubrication, otherwise their functionality cannot be guaranteed and their service life will be shortened. Lubricants such as oil or grease may be used for lubrication. This article explains which lubricant is suitable for which reasons and how to optimally lubricate ball screws.

10 Minutes read

Test equipment and positioning elements for sheet metal parts

In this blog article, we will take a closer look at test equipment and positioning elements for sheet metal parts, explain their significance for production quality and examine their application in mechanical engineering. Quality control of sheet metal parts is crucial for ensuring product quality and customer satisfaction. Precision and accuracy are essential in mechanical engineering and special machine construction. Test equipment such as test pins, positioning bushings and other high-precision positioning elements are used here, which enable an effective and reliable check of the manufactured parts.

7 Minutes read

Cam followers and roller followers - basic knowledge and intended use

From conveyor systems to robot-controlled production lines, cam followers enable the effortless movement of loads. A smooth process in industrial manufacturing and material handling depends on efficient and precise movement systems. Cam followers and roller followers play a decisive role here. Here, cam followers and roller followers ensure reliable guidance of linear movement. In this blog article, we dive into the basic knowledge of these components and examine their intended utilization in industrial practice.

7 Minutes read

The strongest surface treatments for metals – Indestructible, durable and low-maintenance

The choice of the right surface treatment depends largely on the requirements placed on the surface. There are a number of different surface treatments that can be used depending on your needs. In this blog article, we present the strongest, hardest and most durable surface treatments.

4 Minutes read

Metals and surface treatments – An overview

Industrial surface treatment is a process in which the surface of a workpiece is machined to improve or change its mechanical, chemical or visual properties.

7 Minutes read

Damping materials in mechanics and construction: ideas, applications and advantages

Damping materials are essential in mechanics and construction. They are used to absorb shocks and vibrations and to improve the operation of machines and systems. Due to their unique properties, they can be used in various mechanical and technical applications.

8 Minutes read

Types, properties and utilization of retaining rings

The retaining ring is one of the most important tools in construction. It is used to secure individual components and prevent axial movement. In this article, we will take a look at the different types of retaining rings, their features and their utilization.

3 Minutes read

Plain bearings in practice: selection and assembly

Plain bearings are a type of bearing used in machines to facilitate the movement of shaft and bearing. They are also referred to as plain shells, plain bearing bushes, plain bearing sleeves or plain bearing sheaths.

8 Minutes read

Manual locating units – Precision in small spaces

Locating units play a central role in mechanics and are essential for designers in many different applications. In this article, we will review how locating units, their different types and their applications work.

7 Minutes read

Parallel keys and tapered keys – Standards and norms

Parallel keys and tapered keys are two common connecting elements in the mechanical engineering industry. They are used to create a force-locking connection between two components. In this article, the two key types are examined in more detail and their areas of application are explained.

7 Minutes read

Retaining rings C-Type – Purchasing guidelines

Retaining rings are an important component of many machines and systems that serve to secure bearings, shafts, bolts and other components. A commonly used type of retaining rings is type C, which is manufactured according to the Japanese standard JIS. In this article, you will learn more about retaining rings C-type and the Japanese standard JIS.

9 Minutes read
Image - Slotted coupling with encoder

Transmission of rotational movements – Basics of couplings

When shafts and axes are coupled in a machine, there is always a misalignment between the centre points of the shafts. The coupling compensates for this alignment error by the elasticity of the component or mechanical element during rotation or power transmission. Whether you are an experienced engineer or just diving into the world of mechanical engineering, this article gives you a comprehensive insight into the basics of couplings.

4 Minutes read
Picture of a solid shaft

Benefits of precise linear movements: everything about linear shafts

Linear shafts are becoming increasingly popular in drive technology. They offer a high degree of precision in movement. Linear shafts have several advantages compared to traditional shafts, including high rigidity, high positioning accuracy, longer lifetime and also excellent control performance.

19 Minutes read

Shaft couplings – Basics and application areas

This blog article provides an introduction to how couplings work and the different types used today.

6 Minutes read

Friction and friction coefficient determination of friction values of materials

The friction coefficient is a physical variable derived from the field of tribology for the friction between two objects. The friction coefficient sets the force that occurs during friction (frictional force) in relation to the force with which the objects are pressed together (pressing force). The friction coefficient is thus an important parameter when examining material wear and sliding properties. This article explains the basics of the friction coefficient, its measurement methods and its applications in technology.

9 Minutes read

Pipe threads – Standards and standard dimensions

This article examines the standard dimensions of pipe threads and their meaning. Pipes with threads ensure a safe and tight connection between pipe parts and adjacent components. In industry, there are a variety of standards for this, such as DIN/ISO, JIS, BSP, NPT or BSW.

10 Minutes read

Tension pins – Overview design and application

Tension pins, or spring pins are mechanical fastening elements made of spring steel. These elements join components safely and reliably while offering a certain degree of flexibility. They are easy to install and provide even load distribution across the surface of the pin and bore hole. They are widely used in many industries and applications and are particularly useful in applications where a permanent connection is required without the use of screws or other fasteners.

9 Minutes read

Torsion: How to understand torsion

There are many different types of mechanical loads that affect an object, one of which is torsion. In this blog article, we will look at the basics of torsion and explore some examples.

4 Minutes read

Comparison of steels in mechanical engineering with other standards such as JIS and AISI

There are different designation systems for the properties of steel. The underlying standards form the basis for the classification and designation of steel grades using material numbers. In this article we compare the steel grades classified according to DIN/EN/ISO with their respective counterparts in JIS (Japanese Industrial Standard).

7 Minutes read

Calculate different gear units – The most important formulas for gear drives

Since it is of great importance in the design of gears that the gear wheels involved engage correctly and wear is minimized, various basic calculations must be carried out. Terms such as modulus, pitch diameter and tooth count play a major role here. In this article, we deal with the most important aspects of gear calculation and what to consider when calculating gear units.

8 Minutes read