RETAINERS

Type Shape Locating method Mounting method
For round punch / die Type For shaped punch Type Retainer
body
thickness
Heavy duty type for high-tensile steel
End retainers for NC machining HDP-AP
HDPAR
BPC
HDP-AN
HDP-FP
HDPFR
BPC
HDP-FN
30 Punch locating is performed by means of the two dowel holes in the retainer. Bolt is inserted from the punch tip side, fastening the retainer to the die.

End retainers for NC machining
-For heavy load-
HAP-AP
HAPAR
BPC
HAP-AN
HAP-FP
HAPFR
BPC
HAP-FN
35 Punch locating is performed by means of the two dowel holes in the retainer.
Square retainers HSR-AP
HMPSR
MPSP
HSR-AN
HSR-FP
HMPDR
MPSP
HSR-FN
30 Punch locating is performed by means of the two dowel holes in the retainer.
Square retainers
-For heavy load-
HSA-AP
HASAR
MPSP
HSA-AN
HSA-FP
HASAR
MPSP
HSR-AN
35
Single fixing-bolt type
End retainers for NC machining SP-APS
SPARS
BPST
SP-ASN
SP-FPS
SPFRS
BPST
SP-FSN
25 Punch locating is performed by means of the two dowel holes in the retainer. Bolt is inserted from the punch tip side, fastening the retainer to the die.

End retainer for edge-matching machining TP-APS
TPARS
BPST
TP-ASN
TP-FPS
TPFRS
BPST
TP-FSN
25 Punch locating is performed by machining a matching hole at the retainer dowel hole after the edges of the punch and die have been matched. (Note 1)
Double fixing-bolts type
End retainers for NC machining DP-AP
DP-AD
DPAR
BPC
BDC
DP-AN
DP-FP
DP-FD
DPFR
BPC
BDC
DP-FN
30 Punch locating is performed by means of the two dowel holes in the retainer. Bolt is inserted from the punch tip side, fastening the retainer to the die.

End retainer for edge-matching machining CP-AP
CP-AD
CPAR
BPC
BDC
CP-AN
CP-FP
CP-FD
CPFR
BPC
BDC
CP-FN
30 Punch locating is performed by machining a matching hole at the retainer dowel hole after the edges of the punch and die have been matched. (Note 1)
End retainers for NC machining
-For heavy load-
AP-AP
APAR
BPC
AP-AN
AP-FP
APFR
BPC
AP-FN
30 Punch locating is performed by means of the two dowel holes in the retainer.
End retainers for edge-matching machining
-For heavy load-
FP-AP
APAR
BPC
AP-AN
FP-FP
FPFR
BPC
FP-FN
30 Punch locating is performed by machining a matching hole at the retainer dowel hole after the edges of the punch and die have been matched. (Note 1)
Triangle type
End retainers for NC machining 25CRN-AP
25CRN-AD
25CRNAR
CRNBP
CRNBD
25CRN-A
25CRN-FP
25CRN-FD
25CRNFR
CRNBP
CRNBD
25CRN-F
25
32
Punch locating is performed by means of the two dowel holes in the retainer. Bolt is inserted from the punch tip side, fastening the retainer to the die.

CRN-AP
CRN-AD
CRNAR
CRNBP
CRNBD
CRN-A
CRN-FP
CRN-FD
CRNFR
CRNBP
CRNBD
CRN-F
Square type
Square retainers SR-AP
SR-AD
MPSR
MPSP
MDSP
SR-AN
SR-FP
SR-FD
MPDR
MPSP
MDSP
SR-FN
30 Punch locating is performed by means of the two dowel holes in the retainer. Bolt is inserted from the punch tip side, fastening the retainer to the die.

Square retainers
-For heavy load-
SA-AP
ASAR
MPSP
SA-AN
SA-FP
ASFR
MPSP
SA-FN
(Note1) Matching-hole machining: Dowel hole machining without using NC is performed by installing the retainer with punch mounted onto the upper die, aligning the punch and die edges, then using a drill to create a hole while the retainer is attached. A reamer is then used to simultaneously machine the retainer and upper die.
(Note 2) Correct use of end retainers and square retainers
With a square retainer, the punch is inserted at the center of the shape. As a result, this type provides superior balance. However there are many cases in which the holes that will actually be machined in the product are close together and a square retainer cannot be used due to space problems. End retainers are used in such cases when there is insufficient mounting space.

Select retainers Compact air type Standard air type Standard manual type Air type for heavy load
Type SLC-EA
SLC-FA
SLC-SEA
SLC-SFA
SLS-EA
SLS-FA
SLS-SEA
SLS-SFA
SLS-EH
SLS-FH
SLA-EA
SLA-FA
SLA-SEA
SLA-SFA
Stroke ST=8mm ST=10mm
Shaft dia. D=10•13•16•20 D=10•13•16•20•25•32 D=10•13•16•20

TOP